Other Parts Discussed in Thread: AWR1642
I need to use the command UART (UART0) in the AWR1642 booster pack.
This UART is used in the Demo project to connect with the PC COM port via a micro-USB cable.
Then the Demo Visualizer can communicate with the Demo program running within an AWR1642 booster pack.
For some reasons, I want to use this UART to connect my own device now.
I look over the schematic of the booster pack and decide to wire out the PIN 5 (AR_RS232TX) and PIN 7 (AR_RS232RX) in J6 connector to connect to the RS232 connector in my own device.
The signal level is standard RS232 level, not UART TTL level, for the RS232 connector in my own device.
Are they (AR_RS232TX and AR_RS232RX) the correct/good pins for me to connect my own device?
Do I need some extra circuit to change the signal level of AR_RS232TX and AR_RS232RX?
Any suggestions are welcome.
Thanks in advanced.