Hello,
X/Y/Z is in Q format, and Q format depends on the range resolution.
After the experiment, I found that when the range resolution is 0.04, X/Y/Z is expressed in Q9 format; when the range resolution is 0.3, X/Y/Z is expressed in Q7 format; when the range resolution is 0.977, X/Y/Z is expressed in Q5 format. So what is the relationship between Q format and range resolution? Is there any law?