This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDC1000-GASEVM: minimum range issue

Part Number: TDC1000-GASEVM

Hello Team,

One of my customer is using TDC1000-GASEVM (with BSTEVM) to extend the sensing range.

They are using a 1MHz transducer for water level sensing- woth 30V boost enabled to drive UCC devices.

They are getting good results in the range of 10cm to 20cm.

But , if water level is less than 10cm, output of GUI doesnt show it going below 10cm.

What parameters/setting can be focused upon to resolve the issue?

Regards,

Mahendra