This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AFE4403EVM: How to process the result of the SPO2 sensor and the meaning of GUI output, such as LED1, LED1 ambient, LED2/LED3, LED2/LED3 ambient

Part Number: AFE4403EVM

Hi, I bought a AFE4403EVM, and I am able to follow the manual to install the GUI, driver and also obtain some preliminary results. I have some questions regarding the results, please help me, thanks.

When I look at the result from the GUI, it has the LED1, LED1 ambient, LED2/LED3, LED2/LED3 ambient

1. May I ask how do I obtain the SPO2 from these graphs? 

I looked at some documents, R=ACrms of Red/DCred / (ACrms of IR/DCIR), and SPO2=110-(25*R)

2.Also, I am not sure what do the LED1, LED1 ambient, LED2/LED3, LED2/LED3 ambient stands for? Is the LED1 the red LED, LED2 infrared? LED3 Green LED? Does the LED2/LED3 is the voltage of LED2/LED3?

3. I suppose all the results of voltage are from the photodiode output?

4. Why does this Evaluation board has a green LED? According to the manual, the third green LED isenabled with TX3 mode in the TX Stage tab during the measurement.

Thanks in advance!

  • Hi Hao,

    Few answers.
    1) Typically SpO2 is calculated based on some empirical formula. The one mentioned above is one of them. Its the user who decides the formula/algorithm to convert the raw data into SpO2.
    2) You can refer to section 9 of the user guide to find about the LED association with the color for the given sensor board.
    3) Photodiode gives current output, which is converted into voltage by the Trans-Impedance Amplifier and then converted into digital codes by ADC.
    4) Some user use Green LED for heart rate measurement.

    Regards,
    Prabin