Other Parts Discussed in Thread: AWR1243
Hi everyone,
We are currently working with the AWR1243+DEVPACK+TSW1400EVM. We are now analyzing the raw ADC data and reached to the point of angular estimation(Angle FFT).
In our implementation , we have defined the angle bins by dividing Max.FOV(90 deg)/No. of RX . Since we used only 1 TX and 4Rx for our test data, we now have only 4 angle bins. Hence the step size between the angle bins is very large and we are not able to detect the precise angle for all the cases. Now we are also aware of the fact that, the angle resolution would have been better, if we had configured 2 TX which would have yielded in 2*4= 8 Rx virtual channels. However, we know that radars used in cars can have a small angular spacing/resolution (< 1 deg) even with a 1 TX setup. Is this solution achieved by chirp configuration or by some DSP method?
Thank you in advance for your help!