This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1642: how to deal with raw data in MMW demo?

Part Number: AWR1642

Hi,

I run mmw_dss and mmw_mms by css,and I capture some raw data ( I collected data like that in the picture.). But I don't know how to deal with some data

Can you help me? Thanks

  • Hi,

    This is not the raw data, it is th object data provided by the demo

    Is this what you intended to capture?

    If yes, please check the demo documentation for the output data format

    Thank you

    Cesar

  • Hi,

    At first I was going to use the capture demo to capture the raw data. But I found it impossible to create a CCS project through capture demo code.

    I run capture demo through *.xe674 and *.xer4f that have been compiled in the F:\ti\mmwave_sdk_01_01_00_02\packages\ti\demo\xwr16xx\capture.

    I can't compile these two files by CCS. Can you give me some help?

    Thanks.

  • Hi,

    First, you should be able to build the capture demo with the included makefile. No need for CCS project

    Then, for debugging, after loading the executables, you can load the src files in CCS and set breakpoints.

    You should not need a CCS project for that.

    If you would like to create a CCS project, please search the forum for "mmwave ccs configspec" . There are several threads similar to the one below

    e2e.ti.com/.../2532025

    Thank you
    Cesar