This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMP116: power ripple issue

Part Number: TMP116


Hi All, I am using the tmp116n chip in a temperature device, but i have a  questions need you help to solve.

In my desgin,the power ripple of the tmp116n is about 300-400mv,and the frequence of the ripple is about 10Hz.so,i want to know dose this ripple may have a bad affect on the tmp116n's accuracy?

Thanks!

  • Hi Matthew,

    Have you provided a bypass capacitor near the TMP116 device? The power situation isn't ideal, but may not be harmful depending on the accuracy you wish to achieve.

    The TMP116 has good power supply rejection as shown in the temperature accuracy table. We offer the highest accuracy at 3.3V. When expanding the supply range to 3.0 to 3.6, we only decrease the accuracy specification by 0.1 typical. There is also an increase in temperature range that plays a role in the accuracy de-rating. Finally, across the whole supply range of of 1.9 to 5.5V, we only decrease accuracy 0.1C further to 0.5C max.

    Thanks,
    Ren
  • Hello Mathew.

    For precise measurements it is better get rid of ripples where they are originated. But another solution is to use a RC circuit in TMP116 supply line. Because TMP116 consumes only 0.13mA you can use resistance like 5-10KOhm and not very big electrolitical cap (10-30uF) to fight 10Hz. If it for some reasons is not possible then you should consider to switch to some averaging mode. The internal averaging for 500mSec (if it is acceptable) should eliminate the ripple effect.

    Regards, Michael