This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/AWR1642BOOST: AWR1642BOOST Rev A doesn't work with DSK 2.0?

Part Number: AWR1642BOOST
Other Parts Discussed in Thread: AWR1443BOOST, AWR1642

Tool/software: Linux

Hello,

I just got an AWR1642BOOST Rev. A. I flashed it with SDK 2.0 successfully, but in "mmWave Demo Visualizer" when I click on "SEND CONFIG TO MMWAVE DEVICE", nothing happens, i.e., there is nothing in "Console Messages". Then I went back to SDK 1.2, after re-flash, it works fine as AWR1443BOOST. Does this mean SDK 2.0 doesn't support AWR1642BOOST Rev. A (I guess it only support Rev. B and up) as it doesn't support AWR1443BOOST. 

I wonder what is it, as my colleague just order another AWR1443BOOST and a AWR1642BOOST, the Rev. B just released last week after our order? I even can't find a document for Rev. A of AWR1642BOOST now. 

I would like the new feature of Rev. B to have a switch for SPI and CAN. Do you have plan to have this switch also on AWR1443BOOST?

Best Regards,

Tao Wang