This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/AWR1642BOOST: Sensor will not work, if I create a CAN-FD task to receive CAN-FD status.

Part Number: AWR1642BOOST


Tool/software: TI-RTOS

Hi,

I want to integrate CANFD test code into SRR demo code.

I already verifyied the CANFD test code. (C:\ti\mmwave_sdk_01_02_00_05\packages\ti\drivers\canfd\test\xwr16xx)

Now, I copy "mcanEVM_EVMTest" function to SRR demo code.

And I create "mcanEVM_EVMTest" as a task and then start the sensor, there is no data output in Matlab demo UI.

Do you have any idea for it?

Thanks.