hi,
How should OPT8241EVM calibrate camera parameters be set? Such as duty cycle, LED peak power, etc.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hi,
How should OPT8241EVM calibrate camera parameters be set? Such as duty cycle, LED peak power, etc.
Hi Eric,
Calibration parameters for the OPT8241EVM include lens calibration, phase offset correction, etc. Do you mean how do we set these parameters?
Please refer to the section 7.3.8 of the OPT9221 datasheet.
For duty cycle, refer to section 7.3.3.5.
Suramya
Eric,
I've attached the checkerboard image. Please note that the pattern counts just the inner points of the checkerboard, and the size of this is 10*15