This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1642: IWR1642 vs IWR1443

Part Number: IWR1642
Other Parts Discussed in Thread: IWR1443, , , IWR1443BOOST

Hi,
What is the most suited component (IWR1642 or IWR1443) for each of the following task:

  1. Send (e.g. through SPI or I2C) the range and angles of the 10 closest point.
  2. Send (e.g. through SPI or I2C) the position (relative to the sensor) of all the detected points.
  3. Do an iterative closest point (ICP) between each pointcloud of each frame and send the resulting rotation and translation (e.g. through SPI or I2C).

Many thanks,
Alex