This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AFE5808: Noise question of AFE5808

Part Number: AFE5808


Hello TI Experts,

I am using AFE5805A to do Ultrasonic analog front-end signal processing.

I find that the static noise between channels is quite different~

Test conditions:HDL6M05585 keeps the input state all the time,128 ultrasonic input channels all to ground,

                          ADC sample clock 50MHz,FPGA does sample acquisiation to 0-63 channels,then use Matlab to analyze the data

Question:The input is all to ground,why there's such a big difference in the two sampling value of ADC?

              Such as the pictures below:

Picture1:0-63 channels ,static noise,rms value (ADC)

Picture2:0-63 channels,static noise,Parallel display in time domain,


Picture3: 55th channel amplification


Picture4: 0th channel amplification

Hope for your reply,thank you very much~