Other Parts Discussed in Thread: MMWAVE-SDK,
Hello,
This si Fady Aziz, Fraunhofer IPA, Germany.
I am now trying to get started with the IWR 1642 BOOST and I am lost with searching too much the last two days.
I have followed the steps here in this video:
ti.com/StartIWR1642
It is now connected correctly and I can see it in Com ports in Windows,
Then after that I have tried to use this link:
dev.ti.com/mmWaveDemoVisualizer
It is always giving me this message
I have made all teh steps that i can make and unistalled the anti-virus totally from my PC without the problem being solved
I have also received an advice from Customer Support to install CCS v7 and then import the project from there. I have installed but couldn't import and didn't understant what to import.
I have some issues and questions:
1- I need to solve the problem of the online GUI
2- Is there any normal GUI I can install on my PC and run the kit.
3- Is there anyway to connect the sensor through MATLAB?
4- All the demos I have fiund were for IWR 1443 Is there any demos available for IWR 1642 ?
5- Can the demos work for both sensors? I have studied the hardware differences between both radar systems.
Thank You,
Fady Aziz