This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1642: CAN short circuit problem

Part Number: IWR1642


I'm using the IWR1642, and there is a problem about the CAN interface.

When I shorted the CANH and CANL, or CANH and GND, or CANL and VCC, the function of the CAN interface doesn't work any more. However, when the short circuit  doesn't exist, the CAN still can't work due to the previous shorting problem. 

My problem is what can i do (software or hardware) to let the CAN re-enter working status as normal when the short circuit doesn't exist?

Thank you.