Other Parts Discussed in Thread: DRV8870, TDC1000, TDC7200, DRV8837
Hi
I'm looking for an analog front end for a 200 kHz ultrasonic underwater transducer with 50W tone burst drive power. The device must be used for range measurements.
Have been looking at TI's portfolio and especially the PGA460. It seems to have great software to test and configure the IC for optimum operation.
As far as I can see the PGA460 has the option to operate with a high frequency transducer (adjustable between 180-480 kHz with 1.2kHz steps) that gives 200.4 kHz.
However, as far as I can see, the PGA460 is only capable of delivering 7.5W during tone burst (VVPWR_XF = 15V and I_BURST = 500mA).
Do TI have driver ICs that are capable of delivering up to 50W or are there any ways I can make the PGA460 deliver this amount?
Best Regards,
Andreas