Hi Team,
I have a customer planning on using the PGA460 in an ultrasonic distance sensor for robotic applications and have a question they would like to clarify:
The PGA460 data sheet indicates that the DSP frequency accuracy is +/-4%, and this is used as the basis for setting the drive waveform frequency delivered to the ultrasonic sensor. However, piezo ultrasonic transducers generally specify +/-1% frequency accuracy. The datasheet is somewhat ambiguous, but I’m wondering if the PGA460 tunes the actual drive frequency to the resonance peak of the transducer. If not, how does one ensure that the transducer is driven at resonance?
Thanks for the help and insights.
Best regards,
Jerry