Tool/software: TI-RTOS
Hi,
please find inline queries.
Could you please elaborate what you mean by "FOV(Field of view) of AWR1642 boost to be 50 degrees and 15 degrees for short range coverage(80m)."
ans:we want to maintain short range that is 80m but want to limit field of view to be 50 degrees.
Will you develop your custom software or will you be re-using some of the software?
ans: we are using SRR demo code provided by ti on AWR1642 BOOST but want to do software changes to meet above requirement.
Let's assume you will use the OOB SDK demo.
The demo sends (x,y) detected point information for +/-60deg to the host through uart.
It is possible for the host gui to limit display of points only in smaller FOV such as +/-50deg or +/-30deg
ans: yes it is possible in gui.But we want to do it in radar operational level.The reason is,instead of uart,if other interfaces are connected(CAN ..etc) ,Objects beyond 50 deg FOV are still coming in CAN logs. Main objective is to decrease FOV (still maintaing 80m range and without HARDWARE change i.e still using AWR1642BOOST).
Thanks,
K Subrahmaniam