Part Number: DDC112
Other Parts Discussed in Thread: DDC232
Hello.
If the integral time is set to 10ms and the following current signal is measured, can it be measured as the average value?
Repetition cycle: 10ms
Duty ratio: 0.1%
Signal level: The average value is about 50% of the measurement range
Regards,
Dice-K