This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPT3101: Possible mistake in datasheet application design

Part Number: OPT3101

Page 96 of the datasheet, equation 9, states that phiPD is "Photodiode field of view = 20° for SFH213FA". The ambient power that I computed was 1.166 mW/cm2 using the application conditions. The only way I could get the supplied ambient power of 0.2736 mW/cm2 was by using a phiPD of 10 instead of 20. Is this phiPD variable actually FOV, or half angle?

http://www.ti.com/lit/ds/symlink/opt3101.pdf