Hi,
If Range Direction and Doppler Direction are not used,
Are Demo stopped?
I use mmWave Demo Visializer,online.
Platform:xWR14xx
SDK:1.2
Antenna Config:4Rx,2Tx(15 deg)
Range Direction : no checked.
Doppler Direction :no checked.
I push "Send Config to mmw Device",demo stated.
The demonstration started smoothly
I confirme the display of many plots.
But, when I move my hands at random in front of the sensor ,
and the sensor falls. The plots all stopped.
the mmWave Demo Visializer was freezed.
Number of detection Objects :100
(When plots were moving,it's under 10 usualy.)
InterFrameProcessingMargin(usec):about 50000 to 55000
(When plots were moving,it's about 80000 to 85000 .)
Regards,
user5205609