This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compiler/OPT9221: Sequence of writing bit values to register OPT9221

Part Number: OPT9221
Other Parts Discussed in Thread: OPT8241,

Tool/software: TI C/C++ Compiler

Hello TI

We made our ToF board based on your demo-board OPT8241&OPT9221.

My question is: Is it important the sequence of writing bit values to register OPT9221 or not,? (because I can not receive right phase data while calibration process for second frequency )

I know about tg_dis and mod_pll_update, but may be there is something more?

  • // Initialization sequence for OPT9221
    // 
    // RegAddr is (slaveID << 16) + RegisterAddress
    // Translate internally as needed
    // OPT9221_RegWrite(RegAddr, RegValue)
    //
    // The following sequence will bring up OPT9221 with 4 quads, 4 subframes, 9% integration at 20 fps, 48 MHz modulation frequency, no dealiasing
    // and with (1280 bytes * 240 lines) DVP output with horizontal blank period of 1280 bytes
    //
    OPT9221_RegWrite(0x5880, 0x000001);	// tg_dis = 1
    OPT9221_RegWrite(0x5C3C, 0x005000);	// blk_size = 1280
    OPT9221_RegWrite(0x5C3D, 0x005000);	// blk_blank_size = 1280
    									// Configure blk_blank_size as needed by the receiving chip
    OPT9221_RegWrite(0x5C3F, 0x00000A);	// fb_ready_en = 0
    OPT9221_RegWrite(0x5882, 0x0249F0);	// pix_cnt_max = 150000
    OPT9221_RegWrite(0x5C4C, 0x800006);	// intg_duty_cycle = 6
    OPT9221_RegWrite(0x5880, 0x000000);	// tg_dis = 0
    
    // Modulation Frequency settings: default of 48 MHz
    OPT9221_RegWrite(0x580C, 0x100000);	// mod_m1 = 16, mod_m_frac1 = 0
    OPT9221_RegWrite(0x580F, 0x00049A);	// mod_n1 = 2, mod_ps1 = 1
    OPT9221_RegWrite(0x5802, 0x00001C);	// mod_pll_update = 1
    msleep(10);							// 10ms delay - very conservative
    OPT9221_RegWrite(0x5802, 0x000018);	// mod_pll_update = 0
    
    // Optional: Set phy_test_enable to get a deterministic test pattern each frame.
    // This is useful to test the output interface during bringup
    // The test pattern in bytes is 0, 0, 1, 2, 3, ..., 254, 255, 0, 1, 2, ...
    // Note the two leading 0s at the start of the frame
    
    OPT9221_RegWrite(0x5C29, 0x304042);	// phy_test_enable = 1
    // Uncomment the next line to clear it
    //OPT9221_RegWrite(0x5C29, 0x304040);	// phy_test_enable = 0
    
    Semenov,

    It is important to write register values to OPT9221. I've attached an example init sequence.

    Can you send your init settings?

    Suramya

  • Thank you for your answer!

    I have just seen this on forum before.

    In attachment you can see fragment of code with writing register values to OPT9221.

        
        /* some code */
    
        localparam WRITE_TO_OPT_TOF_5C = {2'b01, 7'h5C};
        localparam WRITE_TO_OPT_TOF_58 = {2'b01, 7'h58};
    
    
         /* some code */
    
        init_data[161]  = WRITE_TO_OPT_TOF_58; //tg_dis = 1
        init_data[162]  = {1'b1,  8'h80}; //
        init_data[163]  = {1'b1,  8'b0000_0001}; //
        init_data[164]  = {1'b1,  8'h00}; //
        init_data[165]  = {1'b1,  8'h00}; //    
        
        init_data[166]  = WRITE_TO_OPT_TOF_5C; //
        init_data[167]  = {1'b1,  8'h3C}; //
        init_data[168]  = {1'b1,  8'b0000_0000}; //  blk_size = 1280 (101 0000 0000) 23:4 bit
        init_data[169]  = {1'b1,  8'b0101_0000}; //
        init_data[170]  = {1'b1,  8'b0000_0000}; //
        
        init_data[171]  = WRITE_TO_OPT_TOF_5C; //blk_blank_size = 10 .. 1280
        init_data[172]  = {1'b1,  8'h3D}; //
        init_data[173]  = {1'b1,  8'hC0}; //  hC0
        init_data[174]  = {1'b1,  8'h01}; //  h01
        init_data[175]  = {1'b1,  8'h00}; //   h00    
        
        init_data[176]  = WRITE_TO_OPT_TOF_5C; //
        init_data[177]  = {1'b1,  8'h3F}; //
        init_data[178]  = {1'b1,  8'hFB}; //  FRM_BLANK_SIZE = 15 23:4; fb_ready_en = 1 0:0 bit, fb_ready_pol = 1 1:1 bit
        init_data[179]  = {1'b1,  8'h0}; //
        init_data[180]  = {1'b1,  8'h0}; //    
        
        init_data[181]  = WRITE_TO_OPT_TOF_58; //
        init_data[182]  = {1'b1,  8'h82}; //pix_cnt_max = 133333  (10 0000 1000 1101 0101) 21:0 bit
        init_data[183]  = {1'b1,  8'b1101_0101}; // 
        init_data[184]  = {1'b1,  8'b0000_1000}; //
        init_data[185]  = {1'b1,  8'b0000_0010}; //    
        
        init_data[186]  = WRITE_TO_OPT_TOF_5C; //
        init_data[187]  = {1'b1,  8'h4C}; //  
        init_data[188]  = {1'b1,  8'h12}; // intg_duty_cycle = `18 (12) 5:0 bit, HDR_SCALE = 0 (0) 6:8 bit
        init_data[189]  = {1'b1,  8'h00}; //
        init_data[190]  = {1'b1,  8'b1000_0000}; // STANDBY = false (0) 19:19 bit, STANDBY_PIN_POL = false (0) 20:20, STANDBY_PIN_EN = false (0) 21:21 bit, LUMPED_DEAD_TIME = 0 (0) 22:22 bit, EASY_CONF_EN = true (1) 23:23 bit    
        
        init_data[191]  = WRITE_TO_OPT_TOF_58; //
        init_data[192]  = {1'b1,  8'h0c}; // mod_m_frac1 = 0 (0) 15:0 bit, mod_m1 = 20 (10100) 21:16 bit
        init_data[193]  = {1'b1,  8'h00}; //
        init_data[194]  = {1'b1,  8'h00}; //
        init_data[195]  = {1'b1,  8'b0001_0100}; //
    
        init_data[196]  = WRITE_TO_OPT_TOF_58; //
        init_data[197]  = {1'b1,  8'h0d}; // mod_m_frac2 = 0 (0) 15:0 bit, mod_m2 = 15 (1111) 21:16 bit
        init_data[198]  = {1'b1,  8'h00}; //
        init_data[199]  = {1'b1,  8'h00}; //
        init_data[200]  = {1'b1,  8'b0000_1111}; //
    
        init_data[201]  = WRITE_TO_OPT_TOF_58; //
        init_data[202]  = {1'b1,  8'h0f}; // mod_n1 = 2 (10) 1:0 bit, mod_n2 = 2 (10) 3:2 bit,
        init_data[203]  = {1'b1,  8'b0001_1010}; // mod_ps1 = 1 (1) 6:4 bit, mod_ps2 = 0 (0) 9:7 bit,
        init_data[204]  = {1'b1,  8'b0000_0100}; //
        init_data[205]  = {1'b1,  8'h00}; // MODULATION_HOLD = false (0) 18:18 bit, DEMOD_STATIC_POL = false (0) 19:19 bit, ILLUM_STATIC_POL = false (0) 20:20 bit
        
        init_data[206]  = WRITE_TO_OPT_TOF_5C; //
        init_data[207]  = {1'b1,  8'h02}; //
        init_data[208]  = {1'b1,  8'b0100_0010}; //  ka*ma-kb*mb = 1; ka = 2 (10) 3:0 bit
        init_data[209]  = {1'b1,  8'b0000_1100}; //  f1 = 40MHZ, f2 = 60 MHZ, feff = GCD(f1, f2) = 20, mb = f2/feff = 60/20 = 3 (11) 13:10 bit, ma = f1/feff = 40/20 = 2 (10) 8:5 bit
        init_data[210]  = {1'b1,  8'b1101_0000}; //  dealias_en = true (1) 23:23 bit, ind_freq_data_en = true 22:22 bit
    
        init_data[211]  = WRITE_TO_OPT_TOF_5C; //
        init_data[212]  = {1'b1,  8'h03}; //
        init_data[213]  = {1'b1,  8'b0000_0000}; //  
        init_data[214]  = {1'b1,  8'b0001_1000}; //  DEALIASED_PH_MASK = 3 (10) 14:11 bit
        init_data[215]  = {1'b1,  8'b0001_0000}; //  ka*ma-kb*mb = 1; kb = 1 (1) 23:20 bit
    
        init_data[216]  = WRITE_TO_OPT_TOF_5C; //
        init_data[217]  = {1'b1,  8'hb2}; //
        init_data[218]  = {1'b1,  8'b1010_1010}; //  freq_ratio = f1*4096/f2 = 40*4096/60 = 2730.(6) = 2730 (101010101010) 11:0 bit
        init_data[219]  = {1'b1,  8'b0000_1010}; //
        init_data[220]  = {1'b1,  8'h00}; //
         
        init_data[221]  = WRITE_TO_OPT_TOF_5C; //
        init_data[222]  = {1'b1,  8'h35}; //diods on
        init_data[223]  = {1'b1,  8'h00}; //
        init_data[224]  = {1'b1,  8'h00}; //
        init_data[225]  = {1'b1,  8'b1110_0000}; // ILLUM_MOD_EARLY = true (1) 22:22 bit, ILLUM_EN_EARLY = true (1) 21:21 bit
    
        init_data[226]  = WRITE_TO_OPT_TOF_5C; //
        init_data[227]  = {1'b1,  8'h39}; //
        init_data[228]  = {1'b1,  8'b0000_0000}; //op_clk_freq = 0 (0) 2:1 bit, OP_CLK_EDGE = false (0) 5:5 bit
        init_data[229]  = {1'b1,  8'b0000_0000}; // OP_MODE = 0 (0) 9:8 bit, OP_SERIAL_WIDTH = false (0) 12:10 bit, DEBUG_FRAME_NUMBER_EN = false (0) 12:12 bit
        init_data[230]  = {1'b1,  8'h00}; //
    
        init_data[231]  = WRITE_TO_OPT_TOF_58; //
        init_data[232]  = {1'b1,  8'h83}; //
        init_data[233]  = {1'b1,  8'b0010_0110}; //sub_frame_cnt_max = 2 (10) 7:4 bit, quad_cnt_max = 6 (110) 3:0 bit
        init_data[234]  = {1'b1,  8'h00}; //
        init_data[235]  = {1'b1,  8'h00}; //
    
        init_data[236]  = WRITE_TO_OPT_TOF_5C; //
        init_data[237]  = {1'b1,  8'hb1}; //
        init_data[238]  = {1'b1,  8'b0000_0100}; // MOD_REF_INV = 0 (7-8th bits)
        init_data[239]  = {1'b1,  8'b0101_1110}; // fb_error_cnt_threshold = 10 (A) default (0000_1011) (18:11 bits)
        init_data[240]  = {1'b1,  8'b0010_1000}; // delay_fb_corr_mode = 1 delay_fb_dc_corr_mode = 1
        
        init_data[241]  = WRITE_TO_OPT_TOF_58; //
        init_data[242]  = {1'b1,  8'hbd}; //    init_2 = 310 (1 0011 0110) 21:0 bit, init_4 = true (1) 22:22 bit
        init_data[243]  = {1'b1,  8'b0011_0110}; //
        init_data[244]  = {1'b1,  8'b0000_0001}; //
        init_data[245]  = {1'b1,  8'b0100_0000}; //
    
        init_data[246]  = WRITE_TO_OPT_TOF_58; //
        init_data[247]  = {1'b1,  8'hbe}; //    init_3 = 330 (1 0100 1010) 21:0 bit
        init_data[248]  = {1'b1,  8'b0100_1010}; //
        init_data[249]  = {1'b1,  8'b0000_0001}; //
        init_data[250]  = {1'b1,  8'b0000_0000}; //	
    
        init_data[251]  = WRITE_TO_OPT_TOF_58; //
        init_data[252]  = {1'b1,  8'hbf}; //    init_5 = 3 (11) 23:22 bit
        init_data[253]  = {1'b1,  8'b0000_0000}; //
        init_data[254]  = {1'b1,  8'b0000_0000}; //
        init_data[255]  = {1'b1,  8'b1100_0000}; //
    
        init_data[256]  = WRITE_TO_OPT_TOF_58; //
        init_data[257]  = {1'b1,  8'h0e}; //    sscg_modulation = 0 (0) 9:7 bit, sscg_period = 6 (110) 6:4 bit, sscg_en = true (1) 3:3 bit
        init_data[258]  = {1'b1,  8'b0110_1000}; //
        init_data[259]  = {1'b1,  8'b0000_0000}; //
        init_data[260]  = {1'b1,  8'b0000_0000}; //
    
        init_data[261]  = WRITE_TO_OPT_TOF_5C; //
        init_data[262]  = {1'b1,  8'h04}; // 
        init_data[263]  = {1'b1,  8'h00}; //  sin_f1_q0_coeff = 0 (0) 15:0 bit
        init_data[264]  = {1'b1,  8'h00}; //
        init_data[265]  = {1'b1,  8'h00}; //
    
        init_data[266]  = WRITE_TO_OPT_TOF_5C; //
        init_data[267]  = {1'b1,  8'h05}; //
        init_data[268]  = {1'b1,  8'hFF}; //  sin_f1_q1_coeff = 32767 (7FFF) 15:0 bit
        init_data[269]  = {1'b1,  8'h7F}; //
        init_data[270]  = {1'b1,  8'h00}; //
    
        init_data[271]  = WRITE_TO_OPT_TOF_5C; //
        init_data[272]  = {1'b1,  8'h06}; // 
        init_data[273]  = {1'b1,  8'h00}; //  sin_f1_q2_coeff = 0 (0) 15:0 bit
        init_data[274]  = {1'b1,  8'h00}; //
        init_data[275]  = {1'b1,  8'h00}; //
    
        init_data[276]  = WRITE_TO_OPT_TOF_5C; //
        init_data[277]  = {1'b1,  8'h07}; //
        init_data[278]  = {1'b1,  8'h01}; //  sin_f1_q3_coeff = -32767 (8001h) 15:0 bit
        init_data[279]  = {1'b1,  8'h80}; //
        init_data[280]  = {1'b1,  8'h00}; //
    
        init_data[281]  = WRITE_TO_OPT_TOF_5C; //
        init_data[282]  = {1'b1,  8'h08}; // 
        init_data[283]  = {1'b1,  8'h00}; //  sin_f1_q4_coeff = 0 (0) 15:0 bit
        init_data[284]  = {1'b1,  8'h00}; //
        init_data[285]  = {1'b1,  8'h00}; //
    
        init_data[286]  = WRITE_TO_OPT_TOF_5C; //
        init_data[287]  = {1'b1,  8'h09}; //
        init_data[288]  = {1'b1,  8'h00}; //  sin_f1_q5_coeff = 0 (0) 15:0 bit
        init_data[289]  = {1'b1,  8'h00}; //
        init_data[290]  = {1'b1,  8'h00}; //
                  
        init_data[291]  = WRITE_TO_OPT_TOF_5C; //
        init_data[292]  = {1'b1,  8'h0A}; // 
        init_data[293]  = {1'b1,  8'hFF}; //  cos_f1_q0_coeff = 32767 (7FFF) 15:0 bit
        init_data[294]  = {1'b1,  8'h7F}; //
        init_data[295]  = {1'b1,  8'h00}; //
                  
        init_data[296]  = WRITE_TO_OPT_TOF_5C; //
        init_data[297]  = {1'b1,  8'h0B}; //
        init_data[298]  = {1'b1,  8'h00}; //  cos_f1_q1_coeff = 0 (0) 15:0 bit
        init_data[299]  = {1'b1,  8'h00}; //
        init_data[300]  = {1'b1,  8'h00}; //
                  
        init_data[301]  = WRITE_TO_OPT_TOF_5C; //
        init_data[302]  = {1'b1,  8'h0C}; // 
        init_data[303]  = {1'b1,  8'h01}; //  cos_f1_q2_coeff = -32767 (8001h) 15:0 bit
        init_data[304]  = {1'b1,  8'h80}; //
        init_data[305]  = {1'b1,  8'h00}; //
    
        init_data[306]  = WRITE_TO_OPT_TOF_5C; //
        init_data[307]  = {1'b1,  8'h0D}; //
        init_data[308]  = {1'b1,  8'h00}; //  cos_f1_q3_coeff = 0 (0) 15:0 bit
        init_data[309]  = {1'b1,  8'h00}; //
        init_data[310]  = {1'b1,  8'h00}; //
                  
        init_data[311]  = WRITE_TO_OPT_TOF_5C; //
        init_data[312]  = {1'b1,  8'h0E}; // 
        init_data[313]  = {1'b1,  8'h00}; //  cos_f1_q4_coeff = 0 (0) 15:0 bit
        init_data[314]  = {1'b1,  8'h00}; //
        init_data[315]  = {1'b1,  8'h00}; //
                  
        init_data[316]  = WRITE_TO_OPT_TOF_5C; //
        init_data[317]  = {1'b1,  8'h0F}; //
        init_data[318]  = {1'b1,  8'h00}; //  cos_f1_q5_coeff = 0 (0) 15:0 bit
        init_data[319]  = {1'b1,  8'h00}; //
        init_data[320]  = {1'b1,  8'h00}; //
                  
        init_data[321]  = WRITE_TO_OPT_TOF_5C; //
        init_data[322]  = {1'b1,  8'h10}; //
        init_data[323]  = {1'b1,  8'h00}; //  sin_f2_q0_coeff = 0 (0) 15:0 bit
        init_data[324]  = {1'b1,  8'h00}; //
        init_data[325]  = {1'b1,  8'h00}; //
    
        init_data[326]  = WRITE_TO_OPT_TOF_5C; //
        init_data[327]  = {1'b1,  8'h11}; //
        init_data[328]  = {1'b1,  8'hD9}; //  sin_f2_q1_coeff = 28377 (6ED9) 15:0 bit
        init_data[329]  = {1'b1,  8'h6E}; //
        init_data[330]  = {1'b1,  8'h00}; //
                  
        init_data[331]  = WRITE_TO_OPT_TOF_5C; //
        init_data[332]  = {1'b1,  8'h12}; //
        init_data[333]  = {1'b1,  8'h27}; //  sin_f2_q2_coeff = -28377 (9127h) 15:0 bit
        init_data[334]  = {1'b1,  8'h91}; //
        init_data[335]  = {1'b1,  8'h00}; //
                  
        init_data[336]  = WRITE_TO_OPT_TOF_5C; //
        init_data[337]  = {1'b1,  8'h13}; //
        init_data[338]  = {1'b1,  8'h00}; //  sin_f2_q3_coeff = 0 (0) 15:0 bit
        init_data[339]  = {1'b1,  8'h00}; //
        init_data[340]  = {1'b1,  8'h00}; //
                  
        init_data[341]  = WRITE_TO_OPT_TOF_5C; //
        init_data[342]  = {1'b1,  8'h14}; //
        init_data[343]  = {1'b1,  8'hD9}; //  sin_f2_q4_coeff = 28377 (6ED9) 15:0 bit
        init_data[344]  = {1'b1,  8'h6E}; //
        init_data[345]  = {1'b1,  8'h00}; //
    
        init_data[346]  = WRITE_TO_OPT_TOF_5C; //
        init_data[347]  = {1'b1,  8'h15}; //
        init_data[348]  = {1'b1,  8'h27}; //  sin_f2_q5_coeff = -28377 (9127h) 15:0 bit
        init_data[349]  = {1'b1,  8'h91}; //
        init_data[350]  = {1'b1,  8'h00}; //
    
        init_data[351]  = WRITE_TO_OPT_TOF_5C; //
        init_data[352]  = {1'b1,  8'h16}; //
        init_data[353]  = {1'b1,  8'hFF}; //  cos_f2_q0_coeff = 32767 (7FFF) 15:0 bit
        init_data[354]  = {1'b1,  8'h7F}; //
        init_data[355]  = {1'b1,  8'h00}; //
    
        init_data[356]  = WRITE_TO_OPT_TOF_5C; //
        init_data[357]  = {1'b1,  8'h17}; //
        init_data[358]  = {1'b1,  8'h00}; //  cos_f2_q1_coeff = -16384 (C000) 15:0 bit
        init_data[359]  = {1'b1,  8'hC0}; //
        init_data[360]  = {1'b1,  8'h00}; //
    
        init_data[361]  = WRITE_TO_OPT_TOF_5C; //
        init_data[362]  = {1'b1,  8'h18}; //
        init_data[363]  = {1'b1,  8'h00}; //  cos_f2_q2_coeff = -16384 (C000) 15:0 bit
        init_data[364]  = {1'b1,  8'hC0}; //
        init_data[365]  = {1'b1,  8'h00}; //
    
        init_data[366]  = WRITE_TO_OPT_TOF_5C; //
        init_data[367]  = {1'b1,  8'h19}; //
        init_data[368]  = {1'b1,  8'hFF}; //  cos_f2_q3_coeff = 32767 (7FFF) 15:0 bit
        init_data[369]  = {1'b1,  8'h7F}; //
        init_data[370]  = {1'b1,  8'h00}; //
    
        init_data[371]  = WRITE_TO_OPT_TOF_5C; //
        init_data[372]  = {1'b1,  8'h1A}; //
        init_data[373]  = {1'b1,  8'h00}; //  cos_f2_q4_coeff = -16384 (C000) 15:0 bit
        init_data[374]  = {1'b1,  8'hC0}; //
        init_data[375]  = {1'b1,  8'h00}; //
    
        init_data[376]  = WRITE_TO_OPT_TOF_5C; //
        init_data[377]  = {1'b1,  8'h1B}; //
        init_data[378]  = {1'b1,  8'h00}; //  cos_f2_q5_coeff = -16384 (C000) 15:0 bit
        init_data[379]  = {1'b1,  8'hC0}; //
        init_data[380]  = {1'b1,  8'h00}; //
    
        init_data[381]  = WRITE_TO_OPT_TOF_5C; //
        init_data[382]  = {1'b1,  8'h1F}; //
        init_data[383]  = {1'b1,  8'b0010_0001}; //
        init_data[384]  = {1'b1,  8'b0100_0011}; //
        init_data[385]  = {1'b1,  8'b0000_0101}; //  IQ_SCALE = 0 (0)  22:20 bit
    
        init_data[386]  = WRITE_TO_OPT_TOF_5C; //
        init_data[387]  = {1'b1,  8'hB3}; //
        init_data[388]  = {1'b1,  8'h00}; //  DELAY_FB_COEFF = 2560 (A00)  11:00 bit
        init_data[389]  = {1'b1,  8'h0A}; //
        init_data[390]  = {1'b1,  8'h00}; //
    
        init_data[391]  = WRITE_TO_OPT_TOF_5C; //
        init_data[392]  = {1'b1,  8'h80}; //
        init_data[393]  = {1'b1,  8'h00}; //  PHASE_LIN_CORR_PERIOD = 0 (0) 3:2 bit, PHASE_LIN_CORR_EN = 0 (0) 0:0 bit
        init_data[394]  = {1'b1,  8'h00}; //
        init_data[395]  = {1'b1,  8'h00}; //
     
        init_data[396]  = WRITE_TO_OPT_TOF_5C; //
        init_data[397]  = {1'b1,  8'h81}; //
        init_data[398]  = {1'b1,  8'h00}; // PHASE_LIN_COEFF0_0 = 0 (0) 11:0 bit
        init_data[399]  = {1'b1,  8'h00}; // PHASE_LIN_COEFF0_1 = 0 (0) 23:12 bit
        init_data[400]  = {1'b1,  8'h00}; //
    
        init_data[401]  = WRITE_TO_OPT_TOF_5C; //
        init_data[402]  = {1'b1,  8'h82}; //
        init_data[403]  = {1'b1,  8'h00}; // PHASE_LIN_COEFF0_2 = 0 (0) 11:0 bit
        init_data[404]  = {1'b1,  8'h00}; // PHASE_LIN_COEFF0_3 = 0 (0) 23:12 bit
        init_data[405]  = {1'b1,  8'h00}; //
                  
        init_data[406]  = WRITE_TO_OPT_TOF_5C; //
        init_data[407]  = {1'b1,  8'h83}; //
        init_data[408]  = {1'b1,  8'h00}; // PHASE_LIN_COEFF0_4 = 0 (0) 11:0 bit
        init_data[409]  = {1'b1,  8'h00}; // PHASE_LIN_COEFF0_5 = 0 (0) 23:12 bit
        init_data[410]  = {1'b1,  8'h00}; //
                  
        init_data[411]  = WRITE_TO_OPT_TOF_5C; //
        init_data[412]  = {1'b1,  8'h84}; //
        init_data[413]  = {1'b1,  8'h00}; // PHASE_LIN_COEFF0_6 = 0 (0) 11:0 bit
        init_data[414]  = {1'b1,  8'h00}; // PHASE_LIN_COEFF0_7 = 0 (0) 23:12 bit
        init_data[415]  = {1'b1,  8'h00}; //
                  
        init_data[416]  = WRITE_TO_OPT_TOF_5C; //
        init_data[417]  = {1'b1,  8'h85}; //
        init_data[418]  = {1'b1,  8'h00}; // PHASE_LIN_COEFF0_8 = 0 (0) 11:0 bit
        init_data[419]  = {1'b1,  8'h00}; // PHASE_LIN_COEFF0_9 = 0 (0) 23:12 bit
        init_data[420]  = {1'b1,  8'h00}; //
                  
        init_data[421]  = WRITE_TO_OPT_TOF_5C; //
        init_data[422]  = {1'b1,  8'h86}; //
        init_data[423]  = {1'b1,  8'h00}; // PHASE_LIN_COEFF0_10 = 0 (0) 11:0 bit
        init_data[424]  = {1'b1,  8'h00}; // PHASE_LIN_COEFF0_11 = 0 (0) 23:12 bit
        init_data[425]  = {1'b1,  8'h00}; //
                  
        init_data[426]  = WRITE_TO_OPT_TOF_5C; //
        init_data[427]  = {1'b1,  8'h87}; //
        init_data[428]  = {1'b1,  8'h00}; // PHASE_LIN_COEFF0_12 = 0 (0) 11:0 bit
        init_data[429]  = {1'b1,  8'h00}; // PHASE_LIN_COEFF0_13 = 0 (0) 23:12 bit
        init_data[430]  = {1'b1,  8'h00}; //
                  
        init_data[431]  = WRITE_TO_OPT_TOF_5C; //
        init_data[432]  = {1'b1,  8'h88}; //
        init_data[433]  = {1'b1,  8'h00}; // PHASE_LIN_COEFF0_14 = 0 (0) 11:0 bit
        init_data[434]  = {1'b1,  8'h00}; // PHASE_LIN_COEFF0_15 = 0 (0) 23:12 bit
        init_data[435]  = {1'b1,  8'h00}; //   
    
        init_data[436]  = WRITE_TO_OPT_TOF_5C; //
        init_data[437]  = {1'b1,  8'h91}; //
        init_data[438]  = {1'b1,  8'h00}; // PHASE_LIN_COEFF1_0 = 0 (0) 11:0 bit
        init_data[439]  = {1'b1,  8'h00}; // PHASE_LIN_COEFF1_1 = 0 (0) 23:12 bit
        init_data[440]  = {1'b1,  8'h00}; //
                  
        init_data[441]  = WRITE_TO_OPT_TOF_5C; //
        init_data[442]  = {1'b1,  8'h92}; //
        init_data[443]  = {1'b1,  8'h00}; // PHASE_LIN_COEFF1_2 = 0 (0) 11:0 bit
        init_data[444]  = {1'b1,  8'h00}; // PHASE_LIN_COEFF1_3 = 0 (0) 23:12 bit
        init_data[445]  = {1'b1,  8'h00}; //
                  
        init_data[446]  = WRITE_TO_OPT_TOF_5C; //
        init_data[447]  = {1'b1,  8'h93}; //
        init_data[448]  = {1'b1,  8'h00}; // PHASE_LIN_COEFF1_4 = 0 (0) 11:0 bit
        init_data[449]  = {1'b1,  8'h00}; // PHASE_LIN_COEFF1_5 = 0 (0) 23:12 bit
        init_data[450]  = {1'b1,  8'h00}; //
                  
        init_data[451]  = WRITE_TO_OPT_TOF_5C; //
        init_data[452]  = {1'b1,  8'h94}; //
        init_data[453]  = {1'b1,  8'h00}; // PHASE_LIN_COEFF1_6 = 0 (0) 11:0 bit
        init_data[454]  = {1'b1,  8'h00}; // PHASE_LIN_COEFF1_7 = 0 (0) 23:12 bit
        init_data[455]  = {1'b1,  8'h00}; //
                  
        init_data[456]  = WRITE_TO_OPT_TOF_5C; //
        init_data[457]  = {1'b1,  8'h95}; //
        init_data[458]  = {1'b1,  8'h00}; // PHASE_LIN_COEFF1_8 = 0 (0) 11:0 bit
        init_data[459]  = {1'b1,  8'h00}; // PHASE_LIN_COEFF1_9 = 0 (0) 23:12 bit
        init_data[460]  = {1'b1,  8'h00}; //
                  
        init_data[461]  = WRITE_TO_OPT_TOF_5C; //
        init_data[462]  = {1'b1,  8'h96}; //
        init_data[463]  = {1'b1,  8'h00}; // PHASE_LIN_COEFF1_10 = 0 (0) 11:0 bit
        init_data[464]  = {1'b1,  8'h00}; // PHASE_LIN_COEFF1_11 = 0 (0) 23:12 bit
        init_data[465]  = {1'b1,  8'h00}; //
                  
        init_data[466]  = WRITE_TO_OPT_TOF_5C; //
        init_data[467]  = {1'b1,  8'h97}; //
        init_data[468]  = {1'b1,  8'h00}; // PHASE_LIN_COEFF1_12 = 0 (0) 11:0 bit
        init_data[469]  = {1'b1,  8'h00}; // PHASE_LIN_COEFF1_13 = 0 (0) 23:12 bit
        init_data[470]  = {1'b1,  8'h00}; //
    
        init_data[471]  = WRITE_TO_OPT_TOF_5C; //
        init_data[472]  = {1'b1,  8'h98}; //
        init_data[473]  = {1'b1,  8'h00}; // PHASE_LIN_COEFF1_14 = 0 (0) 11:0 bit
        init_data[474]  = {1'b1,  8'h00}; // PHASE_LIN_COEFF1_15 = 0 (0) 23:12 bit
        init_data[475]  = {1'b1,  8'h00}; //
                  
        init_data[476]  = WRITE_TO_OPT_TOF_58; //
        init_data[477]  = {1'b1,  8'h81}; //
        init_data[478]  = {1'b1,  8'b1010_0000}; //  SLAVE_MODE = 0 (0) 0:0 bit
        init_data[479]  = {1'b1,  8'b0000_0000}; //  SYNC_MODE = 0 (0) 12:12 bit
        init_data[480]  = {1'b1,  8'b0000_0000}; //
                  
        init_data[481]  = WRITE_TO_OPT_TOF_5C; //
        init_data[482]  = {1'b1,  8'h33}; //
        init_data[483]  = {1'b1,  8'b0011_0000}; //
        init_data[484]  = {1'b1,  8'b0000_0000}; //
        init_data[485]  = {1'b1,  8'b0000_0000}; // SYSCLK_IN_FREQ = 0 (0) 23:16 bit
                  
        init_data[486]  = WRITE_TO_OPT_TOF_58; //
        init_data[487]  = {1'b1,  8'h12}; //
        init_data[488]  = {1'b1,  8'b0000_0000}; //  QUAD_HOP_EN = false (0) 7:7 bit
        init_data[489]  = {1'b1,  8'b0000_0000}; //  QUAD_HOP_OFFSET_F1 = 0 (0) 10:8 bit, QUAD_HOP_OFFSET_F2 = 0 (0) 13:11 bit
        init_data[490]  = {1'b1,  8'b0000_0000}; //
                  
        init_data[491]  = WRITE_TO_OPT_TOF_5C; //
        init_data[492]  = {1'b1,  8'h62}; //
        init_data[493]  = {1'b1,  8'h39}; // TILLUM = 57 (39h) 7:0 bit
        init_data[494]  = {1'b1,  8'h00}; //
        init_data[495]  = {1'b1,  8'h00}; //
                  
        init_data[496]  = WRITE_TO_OPT_TOF_5C; //
        init_data[497]  = {1'b1,  8'h63}; //  ?????
        init_data[498]  = {1'b1,  8'b0000_1111}; // DDR_CONTROLLER_FLAG = true (1) 0:0 bit, DDR_CALIBRATION_FLAG = true (1) 1:1 bit, LVDS_PLL_LOCK = true (1) 2:2 bit, MASTER_PLL_LOCK = true (1) 3:3 bit
        init_data[499]  = {1'b1,  8'b0000_0000}; //
        init_data[500]  = {1'b1,  8'b0000_0000}; // OP_OVERFLOW = false (0) 20:20 bit, OP_UNDERFLOW = 0 (0) 21:21 bit, PIX_CNT_MAX_SET_FAILED = false (0) 22:22 bit, INTG_DUTY_CYCLE_SET_FAILED = false (0) 23:23 bit
                  
        init_data[501]  = WRITE_TO_OPT_TOF_5C; //
        init_data[502]  = {1'b1,  8'h61}; //
        init_data[503]  = {1'b1,  8'h36}; // TSENSOR = 54 (36h) 7:0 bit
        init_data[504]  = {1'b1,  8'h00}; //
        init_data[505]  = {1'b1,  8'h00}; //
                  
        init_data[506]  = WRITE_TO_OPT_TOF_5C; //
        init_data[507]  = {1'b1,  8'h51}; //
        init_data[508]  = {1'b1,  8'h00}; // TILLUM_CALIB = 0 (0) 7:0 bit
        init_data[509]  = {1'b1,  8'h00}; // TSENSOR_CALIB = 0 (0) 8:15 bit
        init_data[510]  = {1'b1,  8'b0001_0100}; // DISABLE_OFFSET_CORR = 0 (0) 16:16 bit, DISABLE_TEMP_CORR = 0 (0) 17:17 bit, CALIB_PREC = true (1) 20:20 bit
                  
        init_data[511]  = WRITE_TO_OPT_TOF_5C; //
        init_data[512]  = {1'b1,  8'h40}; //
        init_data[513]  = {1'b1,  8'b0101_0101}; // HD_POL = true (1) 2:2 bit,  VD_POL = true (1) 6:6 bit, 
        init_data[514]  = {1'b1,  8'b0100_0100}; // PHASE_AUX_EN = false (0) 8:8 bit, PHASE_AUX_POL = true (1) 10:10 bit, OP_CS_POL = true (1) 14:14 bit
        init_data[515]  = {1'b1,  8'b0000_0101}; // FE_POL = true (1) 18:18 bit, FE_LAST_CYCLE = false (0) 20:20 bit
                  
        init_data[516]  = WRITE_TO_OPT_TOF_5C; //
        init_data[517]  = {1'b1,  8'h2e}; //
        init_data[518]  = {1'b1,  8'b0000_0000}; // TILLUM_SLV_ADDR = 0 (0) 6:0 bit
        init_data[519]  = {1'b1,  8'b0000_1000}; //
        init_data[520]  = {1'b1,  8'b0000_0000}; //
                  
        init_data[521]  = WRITE_TO_OPT_TOF_5C; //
        init_data[522]  = {1'b1,  8'h36}; //
        init_data[523]  = {1'b1,  8'b0000_0001}; // AMPLITUDE_THRESHOLD = 1 (1) 11:0 bit
        init_data[524]  = {1'b1,  8'b0000_0000}; // SATURATION_THRESHOLD = 0 (0) 23:12 bit
        init_data[525]  = {1'b1,  8'b0000_0000}; //
                  
        init_data[526]  = WRITE_TO_OPT_TOF_5C; //
        init_data[527]  = {1'b1,  8'hb0}; //
        init_data[528]  = {1'b1,  8'h64}; // SENSOR_OVTEMP_THRESH = 100 (64h) 7:0 bit
        init_data[529]  = {1'b1,  8'h5A}; // ILLUM_OVTEMP_THRESH = 90 (5A) 15:8 bit
        init_data[530]  = {1'b1,  8'h00}; //
                  
        init_data[531]  = WRITE_TO_OPT_TOF_5C; //
        init_data[532]  = {1'b1,  8'h27}; //
        init_data[533]  = {1'b1,  8'b0000_0000}; //
        init_data[534]  = {1'b1,  8'b0010_0000}; // PIXEL_DATA_SIZE = 4 (100) 14:11 bit
        init_data[535]  = {1'b1,  8'b0000_0000}; //
                  
        init_data[536]  = WRITE_TO_OPT_TOF_5C; //
        init_data[537]  = {1'b1,  8'haf}; //
        init_data[538]  = {1'b1,  8'b0000_0000}; // DDR_CONTROLLER_INTR_DIS = false (0) 1:1 bit, DDR_CALIBRATION_INTR_DIS = false (0) 2:2 bit, LVDS_PLL_LOCK_INTR_DIS = false (0) 3:3 bit, MASTER_PLL_LOCK_INTR_DIS = false (0) 4:4 dis
        init_data[539]  = {1'b1,  8'b0000_0000}; //
        init_data[540]  = {1'b1,  8'b0000_0000}; // SENSOR_OVTEMP_INTR_DIS = false (0) 18:18 bit, ILLUM_OVTEMP_INTR_DIS = false (0) 19:19 bit, OP_OVERFLOW_INTR_DIS = false (0) 20:20 bit, OP_UNDERFLOW_INTR_DIS = false (0) 21:21 bit
                  
        init_data[541]  = WRITE_TO_OPT_TOF_5C; //
        init_data[542]  = {1'b1,  8'h65}; //
        init_data[543]  = {1'b1,  8'h00}; //
        init_data[544]  = {1'b1,  8'h00}; // ILLUM_FB_ERROR_CNT = 0 (0) 23:12 bit
        init_data[545]  = {1'b1,  8'h00}; //
                  
        init_data[546]  = WRITE_TO_OPT_TOF_5C; //
        init_data[547]  = {1'b1,  8'h66}; //
        init_data[548]  = {1'b1,  8'h00}; //
        init_data[549]  = {1'b1,  8'h00}; // COMP_FB_ERROR_CNT = 0 (0) 23:12 bit
        init_data[550]  = {1'b1,  8'h00}; //
                  
        init_data[551]  = WRITE_TO_OPT_TOF_5C; //
        init_data[552]  = {1'b1,  8'h47}; //
        init_data[553]  = {1'b1,  8'h00}; // COEFF_ILLUM = 0 (0) 11:0 bit
        init_data[554]  = {1'b1,  8'h00}; //
        init_data[555]  = {1'b1,  8'h00}; //
                  
        init_data[556]  = WRITE_TO_OPT_TOF_5C; //
        init_data[557]  = {1'b1,  8'h29}; //phy_test
        init_data[558]  = {1'b1,  8'b0000_0000}; // PHY_TEST_ENABLE = false (0) 1:1 bit, IND_FREQ_DATA_SEL = 0 (0) 3:3 bit
        init_data[559]  = {1'b1,  8'b0100_0000}; //
        init_data[560]  = {1'b1,  8'b0011_0000}; //
    
        init_data[561]  = WRITE_TO_OPT_TOF_5C; //
        init_data[562]  = {1'b1,  8'h3e}; /// 
        init_data[563]  = {1'b1,  8'b1111_0000}; // VD_ACTIVE = 15 4:23bits
        init_data[564]  = {1'b1,  8'b0000_0000}; // 
        init_data[565]  = {1'b1,  8'b0000_0000}; //
        
        init_data[566]  = WRITE_TO_OPT_TOF_5C; //
        init_data[567]  = {1'b1,  8'hb0}; /// 
        init_data[568]  = {1'b1,  8'b0110_0100}; //  sensor_ovtemp_thresh = 100 (01100100) 7:0 bit
        init_data[569]  = {1'b1,  8'b0101_1010}; // illum_ovtemp_thresh = 90 (01011010) 15:8 bit
        init_data[570]  = {1'b1,  8'b0000_0000}; //
        
        init_data[571]  = WRITE_TO_OPT_TOF_58; //
        init_data[572]  = {1'b1,  8'h80}; // tg_dis = 0
        init_data[573]  = {1'b1,  8'h00}; //
        init_data[574]  = {1'b1,  8'h00}; //
        init_data[575]  = {1'b1,  8'h00}; //
        
        init_data[576]  = WRITE_TO_OPT_TOF_58; //
        init_data[577]  = {1'b1,  8'h02}; // mod_pll_update = 1
        init_data[578]  = {1'b1,  8'h1C}; // was init_data[248]  = {1'b1,  8'h1C}; 
        init_data[579]  = {1'b1,  8'h00}; //
        init_data[580]  = {1'b1,  8'h00}; //
        
        init_data[581]  = PAUSE;
        init_data[582]  = PAUSE;
        init_data[583]  = PAUSE;
        
        init_data[584]  = WRITE_TO_OPT_TOF_58; //
        init_data[585]  = {1'b1,  8'h02}; /// mod_pll_update = 0
        init_data[586]  = {1'b1,  8'h18}; //  was init_data[254]  = {1'b1,  8'h18};
        init_data[587]  = {1'b1,  8'h00}; //
        init_data[588]  = {1'b1,  8'h00}; //
    
    
    
    
         /* some code */
    

  • Can you answer something, please?
  • Hi Semenov,

    Please give us some time to review the register settings.

    Regards,
    Subhash
  • Thank you for your answer!
    Regards,
    Semen.
  • sequence and timing seems critical for the writing register values - we are also currently investigating some issues.
    Subash, it would be great if you could come up with a comprehensive description.
  • Can you answer something, please?