Other Parts Discussed in Thread: UNIFLASH, IWR1443,
Hi, I had been able to flash the binary and run against the demo without any problem for three days.
But yesterday when I do an experiments, I observed my mac alerts me "usb accessories disabled for too much power".
My USB port1 can no longer detect the board, so I switched to port2 to continue. (BTW, it does not work when I connect back to port 1 after SMC reset)
Uniflash alerts "not able to connect serial port"
although I could see two com ports are shown on device manager.
SOP is set correctly.
The chip stores SDK demo binaries before not working,
so I also tried the SDK demo visualizer.
After click configure, it shows correct com port, and can get to the state of hardware connected.
But when I send settings to device, the console does not print anything.
Meanwhile, I notice even when USB is not connected, the chip heats badly, way more heated than before.
With the mac alerts, I was wondering if this is because the board or the chip is short-circuited somehow?
How can I verify if the hardware is broken?