Part Number: AWR1642BOOST
Other Parts Discussed in Thread: AWR1642, AWR1443
Hi.
I got problems to use AWR1642 Boost and AWR 1443 Boost.
First, when I use AWR1642, the mmwave demo visualizer said " 'peakGrouping' is not recognized as a CLI command".
Second, when I use AWR1443 Boost, it said " 'cfarCfg' is not recognized as a CLI command".
How can I solve problems and use demo?
Best regards!
Thank you.
mmwDemo:/>% ***************************************************************Skipped
mmwDemo:/>% Created for SDK ver:01.01Skipped
mmwDemo:/>% Created using Visualizer ver:2.0.0.0Skipped
mmwDemo:/>% Frequency:77Skipped
mmwDemo:/>% Platform:xWR16xxSkipped
mmwDemo:/>% Scene Classifier:best_range_resSkipped
mmwDemo:/>% Azimuth Resolution(deg):30Skipped
mmwDemo:/>% Range Resolution(m):0.047Skipped
mmwDemo:/>% Maximum unambiguous Range(m):7.29Skipped
mmwDemo:/>% Maximum Radial Velocity(m/s):20.72Skipped
mmwDemo:/>% Radial velocity resolution(m/s):2.59Skipped
mmwDemo:/>% Frame Duration(msec):111.111Skipped
mmwDemo:/>% Range Detection Threshold (dB):15Skipped
mmwDemo:/>% Doppler Detection Threshold (dB):15Skipped
mmwDemo:/>% Range Peak Grouping:enabledSkipped
mmwDemo:/>% Doppler Peak Grouping:enabledSkipped
mmwDemo:/>% Static clutter removal:disabledSkipped
mmwDemo:/>% ***************************************************************Skipped
mmwDemo:/>sensorStopDone
mmwDemo:/>flushCfgDone
mmwDemo:/>dfeDataOutputMode 1Done
mmwDemo:/>channelCfg 15 1 0Done
mmwDemo:/>adcCfg 2 1Done
mmwDemo:/>adcbufCfg -1 0 0 1 0Done
mmwDemo:/>profileCfg 0 77 7 7 40 0 0 100 1 192 6000 0 0 30Done
mmwDemo:/>chirpCfg 0 0 0 0 0 0 0 1Done
mmwDemo:/>chirpCfg 1 1 0 0 0 0 0 0Done
mmwDemo:/>frameCfg 0 0 16 0 111.111 1 0Done
mmwDemo:/>lowPower 0 0Done
mmwDemo:/>guiMonitor -1 1 1 0 0 0 1Done
mmwDemo:/>cfarCfg -1 0 0 8 4 4 0 2560Done
mmwDemo:/>cfarCfg -1 1 0 4 2 3 0 2560Done
mmwDemo:/>peakGrouping -1 1 1 1 1 255'peakGrouping' is not recognized as a CLI command