This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AFE4405: Load new Settings on AFE4405

Part Number: AFE4405

Hello,

I use the AFE4405 on an external board made by me using the Nordic nrf52 microContoller. With the GUI i have put the Time Settings (Registers) that suits me and saved them.

Now i want to save those Settings/Parameters on my external AFE4405 as Initial Settings, so that when it wakes up it Always have those Settings. If i have to set the Registers with new Values to do this, then which Registers could i Change and which not. In fact, i tried to Initialise all the Registers like i found them in the GUI (under the TAB "Low Level Configuration") but it hasen't work and i think that it is due to some Registers that couldn't/shouldn't be changed.

If you Need more Informations About how i am Using the AFE4405 just tell me and i will be happy to go in the Details. Thanks.