Hi,
I have the OPT8241-CDK-EVM and i feel it is ok for the solution i am working on.
The problem with this solution is the cost of the LEDs that you use, so i have a few questions concerning the use of Hex LEDs that are marked as DNP.
1 - What is the maximum distance we can obtain using the SFH4715S LEDs?
2 - Do they need the diffuser as well?
Thanks,
André Araújo