Hi,
I have observed that when the reflector is placed at around 1.8 meters the 1D-FFT value associated with that bin is around 1.9e4. As the reflector is moved closer, around 40 cms, the 1DFFT value is around 1.05e
An ADC capture was taken of both the above mentioned cases, and the 1DFFT values are plotted on octave. A screenshot of the dump is shown above. There seems to be a decrease in the value of the 1DFFT value as the reflector moves closer.
Why does this happen?. When the reflector is around 1.8 meters the bin is 12(range resolution is around 0.15m) and when the reflector is around 40 cms, range bin is 3..
The profile configuration is as below :
profileCfg 0 77 5 4.3 51.2 0 0 21.53 1 256 5583 0 0 30
Thanks and Regards
Avinash K