I'm looking for an example to modify the sample code which comes with the AWR1642BOOST demo board to add the ability to toggle the output of 1 GPIO based on object detection thresholds, i.e. the relative power in dB (ideally the threshold is set as a config parameter in the header file) and a second GPIO based on the relative distance based on the longitudinal and lateral axis.