Hello,
If i have 9 100K thermistors in parallel the effective resistance is 11.1K. Now the manufacturer datasheet of the 100K thermistor has a table describing the resistance at a specific temperature. If i use the same table the temperature values are incorrect, obviously because 100K is specified at 25 deg C. However if i use the 10K thermistor table from a 10K thermistor datasheet and use those values to compute the temperature of the 100K parallel branch, the values are correct. (The thermistor pull up is 10 K)
Just want to know if this is the right approach ?
This is a continuation from the topic below:
Thanks..