Part Number: TDC1000-TDC7200EVM
Hey,
I'm working with the board TDC1000 & TDC7200 EVM. I use this EVM with a PZT transducer of 3.4 MHz and a reflector to get the concentration of my fluid using the ToF measured and it works perfectly. Knowing that the RX1/TX2 are connected between them. But now i want to use two PZTs one as emitteur and the other one as receiver. I didn't find any documents about how to use two transducers in fluid concentration measurement. So my questions are :
1- Is it possible to use two transducers of 1 MHz up to 3.4 MHz in fluid concentration measurement using this EVM? the distance between the PZTs is 35 mm.
2- What are the configurations that i should do to have a transducer as a receiver only and the other as transmitter?
3- If we can't do this with this board, can i use the TDC1000 gasEVM instead of the first one? how?
Please i need you're help as soon as possible. Thank you