Other Parts Discussed in Thread: IWR1443
Dear support team,
I have a few questions, it will be great if you could kindly clarify them for me.
1. From my understanding the raw data from IWR1443 is processed in MATLAB, is that correct? If so how does the MATLAB read the high speed data without an external device such as TW1400?
2. I read that the heart rate range is between 0.8 Hz - 2 Hz which is approximately between 50 - 120 beats per minute. Is it possible to extend the range to 0.7 Hz - 2.5 Hz by manipulating the code or is there a hardware limitation for HR range?
3. The range bin with the demo is set at 1m and I would like to detect heart rate at 6m. I was wondering if the signals will be strong enough or will have enough information to extract heart rate? What is the maximum distance in which the IWR1443 can detect the HR?
Your help will be much appreciated. Thank you.
Kind regards,
Khalid