This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1443: Is there any way to get the complex range profile over UART by mmw demo?

Part Number: AWR1443

Hi all, 

Is there any way to get the complex samples of the range profile from all antennas via UART in mmw demo? In the packet structure illustrated in the below file, the range-Doppler map is the log mag matrix which finally gives the magnitude of the received samples, not their phase. I know that for transferring that much of data via UART the frame rate and the frame configuration must be set according to the max speed of UART. Here assume that the frame rate is slow enough to transfer all complex samples of all antennas. I am looking for a way to do that either with mmw demo or anything else rather than using LVDS extension. 

FILE:

8255.mmw Demo Data Structure_8_16.pdf

Best regards,

Mostafa