Other Parts Discussed in Thread: IWR1443BOOST
Hi,
I use DCA1000EVM and IWR1443BOOST in combination,firsttime.
Since there is no LAN cable port on PC, I used VGA / Etherenet Adapter.
With reference to spruik7.pdf and spruij4.pdf, I connected two boards and each cable.
I also confirmed the setting of each switch on the board.
But the PC does not recognize the port of the LAN cable of Etherenet.
Device Manager COM has 4 AP-DevPack-EVM-012 and 2 XDS110.
But there is not any Communication Port(COMX),
Etherenet is enabled. All other USB ports are recognized.
Is the switch setting incorrect?
Static IP Address is setting :192.168.33.30
Windows 10 64bits.
I select software config.
sw1:(It is irrelevant if i select software config,isn't it?)
OFF
OFF
ON
sw2:
LVDS_CAST
ETH_STREAM
1243_MODE
RAW_MODE
SW_CONFIG
Using FPGA configration
SW3:
DC_JACK_5N_IN (I Connect DC/USB ,not J4)
FPGA config switch:
1:down
2:up
3:down
4.up
Regards
user5205609