This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DCA1000EVM: Is DCA1000EVM real-time processing?

Part Number: DCA1000EVM


Hi,

(Perhaps I am misunderstanding it?)

When I attach DCA1000EVM to IWR1443BOOT ,can this sensor display the points on the screen in real time?
Or can I only reproduce the datas after a certain time correction?

I did the operation on page 7 of DCA 1000 _Quick_Start_Guide.pptx ,
and confirmed until the screen of 8 pages was displayed.
In my image, the screen of 8 pages would move in real time and display the points as soon as possible.

I have looked at mmwave_studio_user_guide.pdf, but since I do not yet know how to change the parameters,
I'd like to display the points in the default settings.
I clicked on "SetUp DCA 1000" to try and connect, but error.

Do I need to change the SOP jumper or press the reset button on the board?

Regards,
user5205609