Other Parts Discussed in Thread: IWR1443
If the pin P7 of IWR1443 is not used and be left it open (not connect to any where), what could happen? this is NERR_IN pin and it is High_Z state.
Thanks,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
If the pin P7 of IWR1443 is not used and be left it open (not connect to any where), what could happen? this is NERR_IN pin and it is High_Z state.
Thanks,
Hi Feng,
The recommendation is to add pullup resistor to prevent the pin from floating at any point.
Regards,
Charles O
Feng,
I won't expect the boards to fail because the pin is left floating. It can however result in false data on the line.
do you have a IWR1443 that isn't working?
Regards,
Charles O