Other Parts Discussed in Thread: AWR1642,
As title,
If I want to evaluate the AWR1642 EVM board performance versus temperature, what can be the temperature operation range?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
As title,
If I want to evaluate the AWR1642 EVM board performance versus temperature, what can be the temperature operation range?
Hi Cesar,
Sorry that what I need is the AWR1642BOOST EVM board operating temperature, not the silicon..
Hi Cesar,
I found it in AWR1642BOOST user guide: AWR1642 Evaluation Module Single-Chip mmWave Sensing Solution User's Guide (Rev. B), http://www.ti.com/lit/ug/swru508b/swru508b.pdf
The chapter 7 has one note of the operation temperature range below,
NOTE: The AWR1642BOOST has been tested in the 76- to 77-GHz band (2 Tx at a time) at a
maximum peak power of 26 dBm EIRP, and in the 77- to 81-GHz band (1 Tx at a time) with
maximum peak power of 21 dBm EIRP across the temperature range of –20°C to +60°C.
BR, Jesse.