Other Parts Discussed in Thread: AWR1443BOOST, AWR1443
Hi mmWave team,
I am stuck on the following screen when attempting to use mmWave Studio with my DCA1000EVM connected to a AWR1443BOOST. I am able to successfully reset and connect to the COM Port but there appears to be an issue with loading the needed Firmware labeled BSS FW and MSS FW. The process of loading BSS FW completes in a reasonable amount of time but attempting to load MSS FW causes the program to get stuck displaying "0% Downloading Firmware to device... Please wait, you can't terminate". There is no evidence that anything is actually loading while this is displayed and nothing appears to happen when window is closed and reopened.
What can be done to ensure that both BSS FW and MSS FW are loaded correctly?