This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDC7201: part operation temperature

Part Number: TDC7201


Hello,

The Datasheet indicates an ambient max temperature of 85 C and a max Junction of 85 C. Usually the junction is higher than the ambient. The absolute Max junction is 125C.

1. Did TI intentionally rate the recommended junction temperature as 85C or should this be 125C? 

2. in our application the ambient can be 85C but the PCB can also be higher. What is the maximum Junction the device can safely operate at?

Looking at other components Junction temperatures are usually much higher than 85C usually max 100 to 125C with no issues.

Thanks

Adam