Other Parts Discussed in Thread: IWR1642, TIDEP-0091
Tool/software: Code Composer Studio
Hi everybody,
I have a battery application with IWR1642BOOST, I found a very interesting and useful thread on this issue and I follow with full success:
However now I have a doubt about the timers of the system.
I have a time T1, equal to 340ms, between the enable on of the DCDC converter and the sensorStart command on the device.
I have a time T2, equal to 95ms, between the sensorStart command of the device and the first frame transmitted on UART.
Are these timers values in compliace with what you expect in this application?
If a timer is too long, what could I do to reduce it?
Thanks.
Regards.