This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDC1000-TDC7200EVM: TDC1000-TDC7200EVM time stability issue

Part Number: TDC1000-TDC7200EVM

Dear sir / madam,

I am using your TDC1000-TDC7200EVM with our ultrasonic flow sensor for flow measurement.

The configuration files for the EVM is attached.

I am using a 2” pipe with 2, STEMiNC ultrasonic flow sensors of 1MHz

(Model : SMFM21F1000SS) connected at 45⁰ on opposite ends of pipe facing each other.

The 2” pipe ID is 54.8mm and the ultrasonic path length between the two sensors is 77.5mm.

 

I connected the ultrasonic flow sensor on my test rig with a master electromagnetic flow meter.

My observations during the test were that at 28m3/hr flow rate the expected time difference should be between 196.6ns. But the actual time difference is 140ns with variation in the time of ±20ns. Why is that so? Why the time difference not stable? (Note that I have provided straight lengths of 10D on upstream and downstream.) Same is the case with 21m3/hr, 14m3/hr, 7m3/hr & 0m3/hr.(Kindly find attached log file generated by EVM PC utility for your reference.)

In this regard I would like to seek your valuable guidance.

1.            How can I stabilize the variation in delta T ?

2.            Why is the difference of time observed different from that calculated?

                By adjusting the K factor the flow rate can be adjusted but how to stop the variations in 

time.

Also, note that I have used shielded cable from the sensor to the EVM board.(No loose connections or contact problems observed).

TextFileGraph.xlsx

TDC1000_Config0                         45
TDC1000_Config1                         45
TDC1000_Config2                         12
TDC1000_Config3                         03
TDC1000_Config4                         00
TDC1000_TOF-1                           E0
TDC1000_TOF-0                           1E
TDC1000_Error_Flags                     00
TDC1000_Timeout                         21
TDC1000_Clock_Rate                      02
TDC1000_Conts_Trigger                   00
TDC7200_Config1                         02
TDC7200_Config2                         44
TDC7200_Interrupt_Status                07
TDC7200_Interrupt_Mask                  07
TDC7200_Coarse_Cntr_Ov_H                FF
TDC7200_Coarse_Cntr_Ov_L                FF
TDC7200_Clock_Cntr_Ov_H                 FF
TDC7200_Clock_Cntr_Ov_L                 FF
TDC7200_Clock_Cntr_Stop_Mask_H          00
TDC7200_Clock_Cntr_Stop_Mask_L          00
TRIGGER_UPDATE_FREQ                     0009
TDC_AVG/STDEV_NUM_ELEMS                 000A
SAVE_GRAPH_DATA_TO_FILE                 01
FLOW_MODE_SELECT                        01
Y-SCALE_CENTER                          0032
X-SCALE_RANGE                           0032
MEASURE_RTD1                            01
SAVE_RESULT_REGR_TO_FILE                01
GRAPH_MULTI_STOPS                       01
TDC_SELECT                              00
TEMP_RTD_SELECT                         00
TEMP_RTD_MODE                           00
TEMP_AVG/STDEV_NUM_ELEMS                000A
SAVE_TEMP_DATA                          00
GRAPH_YMAX_DATA                         00000000000000C6
GRAPH_YMIN_DATA                         0000000000000062
TDC1000-HV_DRV_EN1                      00
TDC1000-HV_DRV_EN2                      00
HV_DRV_EN1_Period                       001E
HV_DRV_EN2_Period                       001E
ENABLE_POWER_CYCLE                      00
CLK_FREQ_(1-16MHz)                      8.000000
CLK_SOURCE_SEL                          00
CPU_CLK_FREQ                            05
CPU_CLK_EN                              00
TDC1000-HV_BST_PWR_EN                   00
HV_BST_PWR_EN_Period                    0000
FWD2REV_FLOW_DELAY                      0000
TDC1000-IMPE_MATCH_EN                   00
ENABLE_UART_STREAM                      00
ENABLE_MSP430TIMER_TDC                  00