This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear TI support,
I am using the RadarStudio, and I want to change the ADC Start time Var value in the RadarStudio->SensorConfig->Chirp->Manage Chirp.
I want to set different value for the different chirp.
I have set different parameters for the different ''Chirp No.'' in ChirpManager. but only the configuration parameters in the last line are useful.
There is no detailed description of ChirpManager and ProfManager in document "Radar Studio GUI".
Is there any relevant user's guide.
Thank you in advance for your response.
Xian
Hi Cesar,
I have read this document, and I know that you can configure chirp differently.
I don't quite understand the use of ProfManager in RadarStudio.
When I set "Activate" to load all the different configure, the capture raw data is only the last line configured data.
For example
the ProfManager is
the ChirpManger is
Therefore, The first chirp in the first Frame shouldn't be exactly the same as the second to the ninth chirp in the capture raw data.
but the first chirp is same as the fifth chirp.
This result is the same as configuring "Profile ID" and "Chirp No.9" separately.
Regards,
Xian
Hi Kaushal.
I did as you said, but as soon as I change End Chirp TX, the RadarStudio will report a mistake.
[09:00:55] [RadarAPI]: Status: Passed
[09:00:55] [RadarAPI]: ar1.FrameConfig(0, 9, 100, 10, 40, 0, 1)
[09:00:55] [RadarAPI]: Status: Failed, Error Type: CHIRP USED IN THE FRAME IS NOT CONFIGURED BY AWR_CHIRP_CONF_SET_SB
[09:00:55] [RadarAPI]: MatlabProc Status: Failed
Everything else is default.
Thanks
Xian