Other Parts Discussed in Thread: PGA460
I have the TDC1000-TDC7200EVM and the 1MHz piezo transducer that came with it, and I wanted to measure the TOF in a block of ice in order to determine the speed of sound. To do this I wanted to freeze the transducer directly into the ice. Can this transducer be in contact with the ice, or would this damage it? What would be the best way of protecting it while allowing it to remain in contact with the ice?
Also, what configurations in the GUI would be best for this setup? The distance would be less than 70 cm.