Tool/software: Code Composer Studio
I would like to try running one of the labs from the automotive toolbox (SRR demo) on an AWR1642Boost EVM, which has an ES1.0 chip on it.
I was able to install the current version of the automotive toolbox from the resource explorer, but importing the projects into CCS gives the message that SDK 2.0 is required. However, in the release notes for SDK 2.0, it says that version will only work on ES2.0, not ES1.0. In order to run this demo on my EVM, I think I will need to install the older version of the toolbox, which uses the older SDK version. The problem is that I can't see any way to download version 1.2 of the mmwave Automotive Toolbox. The resource explorer only shows me the most recent version (2.1.2). Is there a place I can get the older version?