Hi all,
I am trying to capture moving targets within 3 meters,like torso movement, using iwr1642boost + mmwave DevPack+TSW1400.
When i program frame duration with a relatively long vualue.like 200ms*200frame or 20ms*1000frame, the radarstudio will error. TSW1400 finished capture before frame ending and nothing was captured by TSW1400. Sometimes i repeat click trigger button it will works as normal, while sometimes it not.
I want to know how to solve this problem. Is this situation a common error?
log output is given in the following.
[10:23:44] [RadarAPI]: ar1.SetupTSW1400()
[10:23:49] [RadarAPI]: TSW1400 set-up complete.
[10:23:52] [RadarAPI]: ar1.StartTsw1400Arm("E:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\PostProc\\adc_data.bin")
[10:23:54] [RadarAPI]: ar1.StartFrame()
[10:23:54] [RadarAPI]: Status: Passed
[10:23:54] Frame start async event received!
[10:24:03] [RadarAPI]: MatlabProc Status: Error Number: 1024
[10:24:03] [RadarAPI]: MatlabProc Status: Error Type:
[10:24:03] [RadarAPI]: TSW1400 capture complete
[10:24:14] [RadarAPI]: Frame Ended
[10:24:14] Frame End async event received!
[10:24:26] [RadarAPI]: ar1.StartTsw1400Arm("E:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\PostProc\\adc_data.bin")
[10:24:26] [RadarAPI]: ar1.StartFrame()
[10:24:26] [RadarAPI]: Status: Passed
[10:24:26] Frame start async event received!
[10:24:46] Frame End async event received!
[10:24:46] [RadarAPI]: Frame Ended
[10:25:01] [RadarAPI]: TSW1400 capture complete