This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1642BOOST: Digitizer Streaming

Part Number: AWR1642BOOST
Other Parts Discussed in Thread: DCA1000EVM,

Hello,

I'm trying to verify that the AWR1642BOOST and the DCA1000EVM are the only hardware pieces required to get up and running with streamed raw ADC data collection on the radar eval kit.

Just trying to make sure I'm not missing anything before making an order...

Thanks!

-Steve

  • Stephen,

    You will need to make sure you have the following equipment in order to get up and running with the AWR1642BOOST and DCA1000EVM:

    - AWR1642BOOST
    - DCA1000EVM
    - 2 power supplies (5V, 2.5A minimum)
    - 2 micro USB cables
    - 1 Ethernet Cable

    TI does not provide the power supplies for these devices. They use a standard 2.1 mm barrel jack.

    Please reply if you have any additional questions.

    Regards,
    Kyle