Dears,
I use the sensor to detect only two reflectors, usually they are placed one meter from the sensor and I use the sensor to detect the change in their angle and position while moving away from the sensor.
However my sensor usually detect all other objects in the room (there are objects also from 0 to 1m)!
I need to change the device configuration to detect only the largest two peaks (which represents my two reflectors)!!
Any advice?
Mit herzlichen Grüßen
FMZ