This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1642BOOST: Clarification on calibration data.

Part Number: IWR1642BOOST

Hello,

               I have been following "Range Bias and Rx Channel Gain/Offset Measurement and Compensation" section of "docs/doxygen/html/index.html" to generate the calibration values. As mentioned in the document, it did generate the measurement value compRangeBiasAndRxChanPhase. I was pleasantly surprised with values being displayed continuously. Just wanted to confirm whether I can pick any one line? If I leave it running some of the values changes considerably after a while (Example: have seen 0.26364 --> 0.14234) .

compRangeBiasAndRxChanPhase -0.0400256 -0.40921 0.36652 -0.35443 0.48981 -0.37335 0.40387 -0.48288 0.36081 -0.65350 0.30344 -0.71582 0.55194 -0.71973 0.44095 -0.96472 0.26334
compRangeBiasAndRxChanPhase -0.0400261 -0.40988 0.36566 -0.35507 0.48776 -0.37418 0.40247 -0.48370 0.36008 -0.65280 0.30405 -0.71655 0.54895 -0.71979 0.44012 -0.96564 0.25989
compRangeBiasAndRxChanPhase -0.0400188 -0.40704 0.36914 -0.35187 0.49243 -0.37112 0.40610 -0.48083 0.36441 -0.65060 0.30872 -0.71423 0.55685 -0.71692 0.44662 -0.96304 0.26935
compRangeBiasAndRxChanPhase -0.0400207 -0.40729 0.36661 -0.35300 0.48938 -0.37213 0.40372 -0.48138 0.36206 -0.65250 0.30579 -0.71548 0.55322 -0.71732 0.44318 -0.96463 0.26364

Many Thanks,

Tony