Hello,
I know that currently the AWR devices support up to 4 unique profiles. The profile indices supported in the ICD go from 0 to 3.
For customers who may need to support to more than 4 types of waveform profiles, is it possible to expand the number of profiles to 6 or more ? I understand that at power-up all the four profiles can be loaded up, but during operation of the radar if a new profile is needed then new profile, chirp and frame configs will need to be sent to AWR via SPI which increases timing overhead.
Thanks
RJ