To install the drivers for mmwave-devpack, as per the following file, "training.ti.com/mmwave-sensor-raw-data-capture-using-tsw1400-board", the drivers should be installed from the C:\ti\mmwave_dfp_00_07_00_04\rf_eval\ftdi folder.
However, in the user guide, it is mentioned that the drivers should be installed from the mmwave SDK package.
I have installed the drivers from mmwave SDK package and they are correctly installed (Com ports are assigned)
Is there any difference in the drivers of these two locations?
Thanks.