Other Parts Discussed in Thread: UNIFLASH, SYSBIOS, MMWAVE-SDK, AWR1443BOOST
Tool/software: Linux
"mmWave LAB Object Data Over CAN" lab demo in "mmwave_automotive_toolbox_2_1_2".
I am trying the mmWave LAB Object Data Over CAN. Before I get a PCAN cable, I setup the system to work with NVidia TX2 which has a CAN port. The system I use is Ubuntu 16.04, the code uses CAN Socket. Anytime when reading the socket, always return -1. Connected to a oscilloscope, I cannot see a CAN signal (see attached, the pulse is only 20mv). I had followed the instructions in section 2.3.3 of document swru508b.pdf to populate R11 and R12 resisters with 0 Ω; and removes R4, R6, R28, and R63 resistors.