Other Parts Discussed in Thread: AWR1642
Tool/software: TI C/C++ Compiler
Hi
My company has developed BSD radar application using AWR1642 EVM and has some question as follow:
1. We did road testing and found a problem as following: when a car moved toward our implemented radar and got close enough, with velocity approximated our car’s velocity (the relative velocity approximated zero), then the tracking output on GUI started flashing. Is there any mechanism in the algorithm which eliminate target with small R or with v approximates zero?
2. We see the 15 degrees angle resolution in TI DEP-0092 documents and wonder how it is calculated. If we do 32 points FFT on antennas’ outputs, shouldn’t we get a better angle resolution to be 180/32=5.625 degrees? Why’s the resolution gets worse? If using chinese remainder theory to extend max velocity, we only find the first peak when doing angle estimation, so when two objects has same range and velocity, we can not distinguish two objects in angle domain, right ?(usually call "overlapping issue" in DSP)
3. The same in the documents, we see that the time duration of SRR subframe to be 30 ms, but a set of slow and fast chirps should only takes 8.3 ms. Are there multiple sets of slow and fast chirps transmitted in a SRR subframe? If so, how many of them, and how do they work?
4. Is there hard detection interval, ex: In range 0~80m with peakgrouping only find peak to range bins up to (224)? What is the interval of angle ? Is positive and negative 60 degree of y axis (broadside)?
Best regards,
Henry Lin